Cancel
Showing results for 
Search instead for 
Did you mean: 

Copied parts ST9

Experimenter
Experimenter

Why when I edit a piece copied the original part is also affected? How to let independent?

17 REPLIES 17

Betreff: Copied parts ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

 

copied in which way?

 

 

regards
Wolfgang

Betreff: Copied parts ST9

Honored Contributor
Honored Contributor

I use that to my advantage often. Since I use "resizable" sheet metal. I often insert another copy of a sheet metal part. When changes happen to one, they also happen to the other.

 

If you want a copy of a static part to modify, make sure to name it something different. Then it becomes it's own part.

Betreff: Copied parts ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

I never ever have seen anything that the "name" of a part has to do with wether it changes or not if modifiying an original part.

 

Can You explain, what You are using here.

 

There is only one setting/option I know to define wether or not an interpart copy is assoziativ or not (and this only is true for traditional parts) and this is found in the interpart options.

But this IMHO has nothing to do what name man is using.

 

20161001_1119.PNG

 

 

 

If this option is on then the interpart copy is assoziative if not it is not.

 

regards
Wolfgang

Betreff: Copied parts ST9

Honored Contributor
Honored Contributor

I messed up while making the vid. Do not have time to remake.

 

The point is, Using another copy of a part with the same name, the parts maintain being identical. Different names, they don't.

 

https://youtu.be/I-5lFSgjUzY

 

Betreff: Copied parts ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't think the name has anything to do with it. I think the fact that you used Windows file explorer to copy it breaks the link. Any part copy (properly copied) with link to file checked can be named macaroni or whatever you like and still follow the original.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: Copied parts ST9

Honored Contributor
Honored Contributor

Using explorer to insert the same name maintained the link. Using explorer  to insert the same part with a different name broke the link. That was the point.

 

Notice how the same name copy changed size and the different name did not using the assembly planes at the end.

Betreff: Copied parts ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not sure why you are surprised by this. It's a different part without the links of the original. The name is immaterial.

And more confusion: Why did you copy F2 to F3/test when F1 seemed to be the part of concern?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: Copied parts ST9

Experimenter
Experimenter

Hi,

 

I'm not copying from Windows Explorer, I just use the move with copy command on the Assembly enviroment.

 

Thans for the comments.

 

Renato.

Betreff: Copied parts ST9

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@RB2, That's the same thing as inserting the same part again in a different location. It's just another instance of the part file, not a "copy" as in another file.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200