Cancel
Showing results for 
Search instead for 
Did you mean: 

Corrupt File

N/A

everytime i download the file it comes up as corrupt when i try to install. like i click on it to open and it says corrupt. please help

8 REPLIES

Re: Corrupt File

N/A
With me it is same. I have low download speed and it stops allways at 1gb.

Re: Corrupt File

N/A
yeah thats whats goin on but i have really fast internet

Re: Corrupt File

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi there,

I suggest you use a download manager for this file...
A must for lower connection speeds/bandwidth....this one works & is free...
http://www.freedownloadmanager.org/download.htm


-
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Corrupt File

N/A
how does it work?

Re: Corrupt File

N/A
okay so i have it downloaded but when i try to add the license file it shows a message saying that i need to close all programs first...i dont have any programs open when i do it

Re: Corrupt File

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Great...most of the way there. Not sure what the "close all programs first" message is all about if you have nothing else running....I suggest a reboot may be in order.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Corrupt File

N/A
still doesnt work. it wont let me use my licence

Re: Corrupt File

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
still doesnt work. it wont let me use my licence



Check that your license file is titled... "SELicense.dat". (need file extensions displayed)
Rename your license file exactly as above, then either use the license wizard, or copy & paste it into the installation folder, (normally) "C:\Program Files\Solid Edge ST4\Program" where it will ask if you want to overwrite the existing...say Yes, and you should be good to go. Start the program as normal.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000