Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Re: Count block occurences

Pioneer
Pioneer

i'm looking for a macro-free solution as it will have to work on a lot of workstations and it will be hard to convince people to add a macro.

 

as I said i can move away from blocks I just need some symbols/items/ojects call them whatever you wish that can be counted

Re: Count block occurences

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi @Imics

 

I am not able to do this in ST 8

Is the block count property available only in ST 9  ?

 

Under Source Type, Table is not available:

 

2016_July_25_02.png

 

Thanks.

 

Regards,

Tushar

 

Re: Count block occurences

Gears Phenom Gears Phenom
Gears Phenom
Hi my Friend,

Ohh no, I think this was introduced in ST7. First you have to place balloons with quantities. After this you have to select Balloon at source type.

BR,
Imics
http://solidedgest.wordpress.com/

Re: Count block occurences

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Got it to work now.  Thank you.

It was there in the video all the time.

Did not watch carefully - my bad Smiley Happy