Cancel
Showing results for 
Search instead for 
Did you mean: 

Crashing of ST7 when part and assy files are opened simaltaneously

Experimenter
Experimenter

Hi,

I have loaded ST7 on my PC yestarday.  

 

I can open part file, assy files individually.  I can open multiple part files or assy files.  

 

But if I open part file when the assy files is already open, the software crashes.  The same is true when vice versa.

 

Pls help

 

 

Kushal

 

7 REPLIES

Re: Crashing of ST7 when part and assy files are opened simaltaneously

Gears Phenom Gears Phenom
Gears Phenom

I see you haven't installed MP1, I don't know if this will be the solution, but it's worth the try.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Crashing of ST7 when part and assy files are opened simaltaneously

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What graphics card and driver are you running?



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Crashing of ST7 when part and assy files are opened simaltaneously

Experimenter
Experimenter
Hi

I have this problem too. Iam using windows 10 technical preview on two machines, but the Solid Edge wont work both.

When i try create or open any par, psm, asm the program is crash, but i can open or create dft.

Notebook: i3-380M, Intel HD, 4Gb RAM
PC: i7-920, AMD HD7850, 6Gb RAM

In the crashlogf
Exeption code: 0xe06d7363
COM error: 0x80020005

"The rollback event cannot allow saving of the active document because the command stack is empty."

Anyone can help me?

Thanks,
MoShE
ST7 MP2

Re: Crashing of ST7 when part and assy files are opened simaltaneously

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

First off, Windows 10 is not supported or released so nothing is gauranteed there.

 

Second, your graphics are not supported.  See the following post for a workaround to the crashing.

http://community.plm.automation.siemens.com/t5/Solid-Edge-Student-Edition-Forum/solid-edge-st7-st6-s...

 



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Crashing of ST7 when part and assy files are opened simaltaneously

Experimenter
Experimenter

Thanks for reply!

 

I know that windows 10 is not supported, I just try it.

I am not appalled, but I asked to see if someone can help. I hope its not problem.
 
I can't see this option page in your comment, because I can't open or create par or asm, but I try config it in AutoConfigure.txt, but nothing.. Smiley Sad
 
Just my notebook graphic card is not supported if i know well. The HD7850 in my PC is supported or not?
 
MoShE
ST7 MP2

Re: Crashing of ST7 when part and assy files are opened simaltaneously

Community Manager Community Manager
Community Manager

We are testing Solid Edge ST8 now with the Windows 10 Technical Preview. We also experienced this crash and resolved it in ST8, so that further ST8 testing could continue.

 

Windows 10 is expected to release late in 2015 - after the Solid Edge ST8 release.

 

Any support of Windows 10 would not be possible until ST9 and possibly an ST8MP.

 

Best regards,

Laura Watson

Solid Edge Product Testing

Re: Crashing of ST7 when part and assy files are opened simaltaneously

Experimenter
Experimenter

Thank you! But if you find any solution for this problem that may resolve it in ST7, please contact me here!

 

Best regards,

MoShE