Cancel
Showing results for 
Search instead for 
Did you mean: 

Create Drawings views in Draft

Experimenter
Experimenter

I have the new free 2d drafting solidedge program and

cant figure out how to make a drafting view on the sheet

1 REPLY 1

Re: Create Drawings views in Draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

You need to create your full size geometry on the "2D Model" sheet [this may not be active by default] This can be activated manually by clicking on the 

 

ST8_DFT_DrawingViews_2DModel.png

 

 

You'll then find the tools you need on your Sketching tab, there is a Drawing Views panel.

 

Normally "Sheet 1" [+ additional sheets you create] are your "Working" sheets, these are where you place your model views & then your annotations [dimentions, notes, etc] using the "2D Model" & "Detail" functions

 

ST8_DFT_DrawingViews_2DModel.png

 

Switch back & forth between using the Sheet tab at the lower left of the graphics window.

 

 

ST8_DFT_2DModel_SheetTabs.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000