Cancel
Showing results for 
Search instead for 
Did you mean: 

Create Hole tolerance compliant to h7 standard fit - GD&T questions

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi All

 

Is it possible to create such annotation automatically 

 

The tolerance value are compliant to h7 standard fit 

 

h7.jpg

4 REPLIES 4

Re: Create Hole tolerance compliant to h7 standard fit - GD&T questions

Automatically not, you can do it via PMI in 3D and get the dimensions to draft.

Don't know if it updates after a tolerance change.But I don't know another options to make this an automatic tolerance.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Create Hole tolerance compliant to h7 standard fit - GD&T questions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is this what you mean?

 

htols.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Create Hole tolerance compliant to h7 standard fit - GD&T questions

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I was aware of h7 annotation standard in Solid Edge, but I was thinking whether it can be combined with %HC (Hole callout)

 

To annotate holes, we will usually call the dimension with the "hole callout" function in dimension type...but I won't be able to add h7 compliant tolerance inside my hole callout..

Re: Create Hole tolerance compliant to h7 standard fit - GD&T questions

Is this what you mean?

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10