Cancel
Showing results for 
Search instead for 
Did you mean: 

Create a flat pattern from an a extruded part?

Experimenter
Experimenter

I have a formed part that was created in Solid Edge from a .DXF file (using the "create 3D" command). Now, I'm needing to create a flat pattern (with bend lines shown) for the part to be manufactured.

 

The flat pattern command does not recognize any of the faces on the part. I am only able to create a blank body flat plate. Any ideas on how to show the bend lines? 2D draft only is okay.

2 REPLIES 2

Re: Create a flat pattern from an a extruded part?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @k3vnR,

 

For that functionality to work, Solid Edge expects the model to be in the Sheet Metal environment, and "converted" via the "Thin Part to Sheet Metal" command, so that it can be restructured a sheet body. You may need to "Rip" certain edges to to allow it to develop out.....hard to say what you'll need to do, without seeing your part model. HTH.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Create a flat pattern from an a extruded part?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you translate a file in that has a common thickness on all sections, you can convert the part to sheet metal...

 

Convert thin part:

https://docs.plm.automation.siemens.com/tdoc/se/109/se_help/#uid:cnvrtsm1c

 

Convert solid part: 

https://docs.plm.automation.siemens.com/data_services/resources/se/109/se_help/en_US/graphics/graphi...

 



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com