Cancel
Showing results for 
Search instead for 
Did you mean: 

Create a part with fixed constraints

Valued Contributor
Valued Contributor

Dear all,

another newbe question from an ex Inventor user Smiley Very Happy

I have created many parts that are inserted in an assembly in the same manner, think for example to a screw grommets, they have alwasy the same costrains: planar on a surface, aligned on left side and aligned on right side.

I would like to edit o create a part that once inserted on an assemly, it gave me the predifined constraints of that part, instead that I had to edit them every time.

Think for example to a screw, once inserted on an assembly, it ask for axis alignement and the for the offset from the surface.

 

I hope I explained my problem correctly.

 

TIA for answering

4 REPLIES 4

Re: Create a part with fixed constraints

Valued Contributor
Valued Contributor

Well you need to CAPTURE FIT the mates of the component.

 

 

Capture 1.JPG

 

 

 

 

 

 

 

 

 

Select the links that you want predefined

Re: Create a part with fixed constraints

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

hello @Davide_Parolin

 

See this video to know how it can be done:

 

 

~Tushar Suradkar

fb.pngSolid Edge Users Facebook Group

Re: Create a part with fixed constraints

Phenom
Phenom

Also check Duplicate component and Clone component commands while in assembly mode. While in the assembly you can click and drop a bunch (of the same part/assy) at once and there's even some nice AI there. If the parts are flipped, you can also re-flip them.

 

 

Re: Create a part with fixed constraints

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

hjoy schrieb:

Also check Duplicate component and Clone component commands while in assembly mode. While in the assembly you can click and drop a bunch (of the same part/assy) at once and there's even some nice AI there. If the parts are flipped, you can also re-flip them.

 

 


... and not to forget the pattern feature in assembly.

 

If we are talking abput screws, bolts, nuts, etc. so in my mind there belongs a hole feature to them.

And a hole by definition is a pattern to be used for multiplying single items to every hole of the hole feature.

Especially if we talk about a snyc hole feature where several holes can be placed on several planes although belonging to the same feature.

 

 

regards
Wolfgang