Cancel
Showing results for 
Search instead for 
Did you mean: 

Create a part with specific dimensions

Not applicable

I want to draw a part, for instance 2" x 1/4" inch, what is the process? Picks point
and enter the other cordinants? It seems not to be working for me whe I enter numbers
into the X & Y boxes on the line above the drawing.
Kristin
1 REPLY 1

Re: Create a part with specific dimensions

Not applicable

Hi Kristin,
I would suggest you run through the tutorial. It will answer a lot of your basic
questions and some not so basic. It only takes about 20 minutes to run through it
and it got me started. From there I just played around with it and asked questions
on this forum. Have fun with it. It's a great program.
Ed
"Kristin" wrote:
>
>I want to draw a part, for instance 2" x 1/4" inch, what is the process? Picks
>point
>and enter the other cordinants? It seems not to be working for me whe I enter
>numbers
>into the X & Y boxes on the line above the drawing.
>
>Kristin