Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Create a plan in subassembly

Pioneer
Pioneer

Hi guys,

 

This is my project situation: A main assembly with some parts and one subassembly (weldment). I would like to create a sketch on a plan (with edit in place, of the subassembly) distant "x" from the face of a main assembly component.

Actually I can't create the plan. I do this step:

1- Select subassembly, right click to "edit in place"

2 - Select "Sketch"  and select "other plans" 

3 - At this time I'm trying to select the reference face for the distance of the sketch plane but I can't select anything.

Can anyone help me?

Thank you in advance

3 REPLIES 3

Re: Create a plan in subassembly

Phenom
Phenom

You have to activate PEER:

 

 

 

https://docs.plm.automation.siemens.com/tdoc/se/108/help/#uidSmiley Tongueeerloc1c

 

And all the parts concerned have to be acticated.

 

I hope, it helps you further Smiley Happy

 

Yasser

Re: Create a plan in subassembly

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Did you try to use "Shift" before selecting "reference plane"?

 

Here is a short video (it works with sketch too).

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Create a plan in subassembly

Pioneer
Pioneer

Thank you Imics!