Cancel
Showing results for 
Search instead for 
Did you mean: 

Create automatic centerlines without having hidden edges visible?

Legend
Legend

Hello,

 

before ST9 we could use the Automatic Centerlines command to create centerlines of all holes of the drawing view that are parallel to the axis of the drawing view. After updating to ST9, the tool creates centerlines only if the parts have hidden edges visible.

 

I can set hidden edges visible, then create centerlines and then hide hidden edges after that, but is there a way to create centerlines without having to have hidden edges visible in ST9?