Cancel
Showing results for 
Search instead for 
Did you mean: 

Create hole patterns without reducing computer performance.

Good afternoon. I present a drawback by putting patterns of holes in the whole piece, taking time to process the holes. Is there any way to create hole patterns without having this problem?

 

thanks for your help.

20 REPLIES 20

Re: Create hole patterns without reducing computer performance.

Honored Contributor
Honored Contributor

The performance is best if hole patterns are created directly from sketches. As in the pattern is sketched and then use a cut for all the holes in one operation.

Re: Create hole patterns without reducing computer performance.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@12GAGE, How are you going to pattern circles for the hole cuts in a sketch? Also, wouldn't work for this case with a radial pattern anyway.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Create hole patterns without reducing computer performance.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Anyway, @Ruben_Cuellar13, I'm not clear on what problem you are trying to solve or prevent.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Create hole patterns without reducing computer performance.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Ruben_Cuellar13 You might try putting in the pattern in Ordered and see if you can use the Fast option on the Pattern.  That yields a pattern with low overhead but your cylinder that is patterned must be identical and not cross over to another face when patterned.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Create hole patterns without reducing computer performance.

thanks for answering.

 

To resolve. I need to make eleven patterns throughout the piece. But creating those patterns with so many holes takes a lot of time.

The question is if there is a way to avoid this problem?

Can do the exercise with the file that publishes, generating eleven parts throughout the piece.

Re: Create hole patterns without reducing computer performance.

@KennyG I'll try.

Re: Create hole patterns without reducing computer performance.

Honored Contributor
Honored Contributor

You draw the pattern in a sketch. Every cutout. So yeah it's not nearly as easy to get started. But it does reduce the CPU power required. That was the starting question.

Highlighted

Re: Create hole patterns without reducing computer performance.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can't do a pattern in a sketch.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Create hole patterns without reducing computer performance.

Honored Contributor
Honored Contributor

nope, but you can sketch the pattern.