Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Create hole patterns without reducing computer performance.

How could you create a pattern in the sketch?

For the intention is to make eleven patterns throughout the piece.

Re: Create hole patterns without reducing computer performance.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't see how a cut with multiple sketch circles would outperform a pattern. And, of course it wouldn't help the original poster.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Create hole patterns without reducing computer performance.

Honored Contributor
Honored Contributor

Cuts (not holes) from an ordered sketch are the most efficient way to get penetrations through a part or sheet.

 

I thought the limiting factor was that he wanted a more CPU efficient model. To get there, you have the lose the direct pattern association and use a sketched set of cutouts.

 

I use that method often, because then I can see the pattern dimensions while also seeing out faded out parts the pattern effects.

Re: Create hole patterns without reducing computer performance.

@12GAGE

How can you make circular perforations, perpendicular to a cylindrical piece?

Re: Create hole patterns without reducing computer performance.

Gears Phenom Gears Phenom
Gears Phenom

@Ruben_Cuellar13 How long does it take on your PC?

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Create hole patterns without reducing computer performance.

Generating eleven patterns along the piece takes more than 40 minutes.

Re: Create hole patterns without reducing computer performance.

@KennyG 

Work the holes in tidy, and it is certainly much faster but not sufficient.
Creating the pattern on one side and wanting to do symmetry on the other side takes too much time. If you like you can try.
I do not know if there is any kind of hierarchy in operations to avoid these invaders.
To create more hole the file is heavier.

Re: Create hole patterns without reducing computer performance.

Phenom
Phenom

Do you really need every instance of hole - or could you suppress many of them in the pattern sketch, just leaving enough to define them in your drawing.

Patterns with many instances come into the category of "things to be avoided if possible".

I understand some people need them if models are used in manufacturing.

I can't open your file, but the preview shows you have a cylinder with a very large pattern around it. I assume you then want to pattern that several times along the length. I would suggest suppressing a lot of the instances in the first pattern

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Re: Create hole patterns without reducing computer performance.

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Okay, I understand it's a long time but you have tons of holes.

I try give some advice:

  • Don't use holes (as a feature), I suggest using "faceset" (break them)
  • Use half model and build an assy if possible

Patterning takes ~8min on my 5 years old laptop with my workaround.

 

Here is a video:

 

I'm not expert of parasolid, but parallel processing would be very nice similar case like this. I often meet similar chellanges at sheetmetal perforating and etc...

This was my suggestion. Smiley Wink

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Create hole patterns without reducing computer performance.

@beachcomber

I initially need it for visualization. However I remain with the concern of because it takes a lot of time and that another way can be done.