Cancel
Showing results for 
Search instead for 
Did you mean: 

Create in Place Assembly

Experimenter
Experimenter

I am wanting to create a cable assy by using the create in place command but it won't let create any assembly relationships with the top level assembly.  Is there a better way of doing this?

1 REPLY 1

Re: Create in Place Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

By default, when you use Creat In Place, the new part is created and you are placed in the Edit mode for the newly created part.  You have to create the part geometry and you can use peer parts for reference, but when done, you need to close and return to the assembly.  Once there, the part is treated like any other part.  There is an option to Ground the new part which would prohibit new relationships, so that would need to be deleted if it is present.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com