Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating a Wave Spring in Solid Edge

Pioneer
Pioneer

Hi,

 

I need to create a wave spring but I can't quite imagine how to go about doing it.  I would normally just start with an extruded circle but creating the bends of the wave spring escapes me.

 

Can anyone help me getting started? (If surfacing is the answer, I don't know)

6 REPLIES 6
Highlighted

Re: Creating a Wave Spring in Solid Edge

Legend
Legend

This video may help you

 

(view in My Videos)

Re: Creating a Wave Spring in Solid Edge

Pioneer
Pioneer

Thank you.  I can't read the text in your video but I should be able to pick it a part with sometime.  I jus tneed to experiment with it a bit.

Re: Creating a Wave Spring in Solid Edge

Legend
Legend
What are you using to do the yellow highlight on the cursor?

Re: Creating a Wave Spring in Solid Edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@nanan00 wrote:
What are you using to do the yellow highlight on the cursor?

That looks to be a video by @Imics . If so, maybe he'll get this and answer.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Creating a Wave Spring in Solid Edge

Gears Phenom Gears Phenom
Gears Phenom
Hi,

I use Camtasia for recording video.

BR,
Imics
http://solidedgest.wordpress.com/

Re: Creating a Wave Spring in Solid Edge

Legend
Legend
I knew this was your Video... that is why I saved it!