Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Creating a flexible pipe on imported geometry

Experimenter
Experimenter

Hi SE Users,

 

I want to create a flexible pipe. The issue is the model I have is an imported one, not created in Solid Edge. I do not have Xpress route add-in. I tried to approach it using the 3D sketch, but the sweep option does not highlight. I need to connect 2 points by a flexible pipe. 

 

Please see the image attached.

 

Thanks a bunch.

2 REPLIES 2

Re: Creating a flexible pipe on imported geometry

Valued Contributor
Valued Contributor
I think you can do it using keypoint curve under the surface tab. you will need to have reference geometry in your part from the start and end points but then you can create a curve for the hose and sweep the hose along this curve.


CAD/CAE Manager
ST8 MP9

Re: Creating a flexible pipe on imported geometry

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Yes, @Guy_H's suggestion is good and simply.

 

Here is a short video to reproduce steps:

 

BR,

Imics
http://solidedgest.wordpress.com/