Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating an Arc

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

God Morning Everyone,

With this video... The issue today is creating  an arc from a straight arc to a transition arc. The video is a little vague.

Also, the reply button on the email is not working is it locked if so... Are we to send a reply via. post a comment?

http://screencast.com/t/x1tqP06oJYr

 

Thanks Alots

Greg

1 REPLY 1

That is not a trivial shape you are trying to add. You ne...

Phenom
Phenom

That is not a trivial shape you are trying to add. You need to create an enclosed volume to sweep or protrude. As you saw, open-ended sketch segments do not get you what you want. Also, the sketch elements are brown, which signifies their relationships are broken or corrupt, which can happen if you delete or significantly change the surfaces they were originally attached to. You should recreate them.

-Dylan Gondyke