Cancel
Showing results for 
Search instead for 
Did you mean: 

Creating an edge normal to a surface

Genius
Genius

A late happy new year to you all. I have a tricky little problem that I am trying to solve. I am trying to create a solid from 5 surfaces by stitching them together. However I am having difficulty creating the edge shape that I want. The Ruled edge command is the result I want but I need the top edge to be of variable height.

 

I have used 3D sketch and the sweep tools to create a shape that is similar to what I want but cannot get 3D sketch to create a line normal to the surface. I have also tried by creating a ruled surface and then using the contour curve tool. However there is no way to restrain the curve with dimensions. Also I cannot pick where the edge of the base surface goes from concentric to eccentric.

 

The sample I have attached is the sweep version so that you get an idea of the shape I am wanting to produce.

 

I have so far spent a whole day trying to design better, but so far the software is getting the better of me.

 

Any help with this little problem would be very much appreciated.

 

Neil...

3 REPLIES 3

Re: Creating an edge normal to a surface

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello Neil,

here is my attempt to create your desired geometry. I am not sure if this is what you want to create.

 

In my exampe there you can see feature 3D sketch 8, which include two lines normal to your face. I created this using 3D Include command in 3d sketch environment from feature Ruled 4.

Hope this helps you figure it out.

 

Ota

Re: Creating an edge normal to a surface

Genius
Genius

Hi Ota,

 

Although your solution was not what I was looking for, it did allow me to find the solution. I split the surface into sections and placed ruled surfaces on each section the height I wanted. Then used the sweep command to produce the correct shape. Then connected all the surfaces.

 

Attached is the solution.

 

I greatly appreciated your help with this Ota, many thanks for your time.

Re: Creating an edge normal to a surface

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Neil,

you are welcome.

Sometimes it requres the smallest push :-)

 

Ota