Crosshair

Experimenter
Experimenter

How can i turn the crosshair off?How can i turn the crosshair off?

3 REPLIES

Betreff: Crosshair

hawcad 3rd Gear
3rd Gear

Hi @Crosshair

 

 

looks like a graphics card issue.

 

Check for other post regarding graphic driver, graphics setting for SE

nVidia problem and so on.

 

 It might help to change the graphic options from advanced hardware to hardware,

that is from automatic graphic detection (advanced) to graphic card dependend.

 

20170423_2235.PNG

 

 

This might help.

If not then You can turn off the shading when select and the clueing

 

All of these are functions are using the graphic card and can be the reasong for this behaviour.

 

 

BTW what are the specs of Your computer?

 



regards
Wolfgang

Betreff: Crosshair

Experimenter
Experimenter

Hello Wolfgang,

 

this option didn`t work. I have a similar, or maybe the same problem, right here.

My PC is not the best, so what can i do?

 

grafik.png

 

 

 

 

Betriebsystemname    Microsoft Windows 7 Ultimate
Version    6.1.7600 Build 7600
Weitere Betriebsystembeschreibung     Nicht verfügbar
Betriebsystemhersteller    Microsoft Corporation
Systemname    MARIUS-PC
Systemhersteller    MICRO-STAR INTERNATIONAL CO., LTD
Systemmodell    MS-1727
Systemtyp    x64-basierter PC
Prozessor    Intel(R) Core(TM) i7 CPU       Q 720  @ 1.60GHz, 1600 MHz, 4 Kern(e), 8 logische(r) Prozessor(en)
BIOS-Version/-Datum    American Megatrends Inc. E1727IMS.102, 23.11.2009
SMBIOS-Version    2.6
Windows-Verzeichnis    C:\Windows
Systemverzeichnis    C:\Windows\system32
Startgerät    \Device\HarddiskVolume1
Gebietsschema    Deutschland
Hardwareabstraktionsebene    Version = "6.1.7600.16385"
Benutzername    Marius-PC\Marius
Zeitzone    Mitteleuropäische Sommerzeit
Installierter physikalischer Speicher (RAM)    4,00 GB
Gesamter realer Speicher    3,98 GB
Verfügbarer realer Speicher    1,79 GB
Gesamter virtueller Speicher    7,96 GB
Verfügbarer virtueller Speicher    5,37 GB
Größe der Auslagerungsdatei    3,98 GB
Auslagerungsdatei    C:\pagefile.sys

Betreff: Crosshair

Honored Contributor
Honored Contributor

Turn the graphics down. Go to 16 or 32 bit color.