Cancel
Showing results for 
Search instead for 
Did you mean: 

Curves in broken views not editable

Builder
Builder

Hello guys. This is a weird issue.

 

Inside a drafty, as far as I make the sketch for a broken view using just lines or arcs, there's no problem if I have to edit that sketch in the future (for example if the part referenced changes) to adjust the broken view.

 

However, if I use a spline instead of that, I can no longer move or edit it. If I mix the spline with some straight lines, I will be just able to move the end points of the curve, the rest remains fixed, which is annoying.

 

brokenview.png

 

 

For certain drafts, a curved contour for the broken views feels more intuitive, that's why I would loke to solve this, if possible.

 

Any ideas? Thanks in advance!

1 REPLY

Re: Curves in broken views not editable

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Have you tried clicking the 'Modify Profile' button in the Command bar which allows to modify the spline.

 

15-May-14 3-15-13 AM.png

 

~Tushar Suradkar

http://surfandcode.blogspot.in/