Cancel
Showing results for 
Search instead for 
Did you mean: 

Custom Properties

Genius
Genius

Hi All.

 

I am using custom properties to insert text in my drafts.

I have a couple that are out of place (i.e. wrong order).  Is there a way to re-order the list?

12 REPLIES

Re: Custom Properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Can you give an example or a screen shot of what you mean?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: Custom Properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Dazzie

 

 

 

same as @bshand

 

 

Can You better explain what Your request is?

 

 

regards
Wolfgang

Betreff: Custom Properties

Genius
Genius

Hi Guys.

 

Please see attached file.

 

If I want to add a property and move it so that it is in the order that I want.

 

I may want to add Rev D information, if I do it will be at the bottom of the list and I want to move it to below rev C information.

Betreff: Custom Properties

Gears Phenom Gears Phenom
Gears Phenom

AFAIK the order of that list is not customizable... IIRC it is listed in the order created. You MIGHT be able to find and edit the list via the REG but I don't think it's that big of an issue to warrant messing in there REG personally.

MIght suggest a macro that provides a custom UI for properties entry... see screenshot attached


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Betreff: Custom Properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

As @Johnson_BigMatt said that's not controllable being a Windows feature. I almost never use that properties dialog except to delete properties. Generally I use Property Manager to edit properties in SE. Columns there are sortable.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: Custom Properties

Genius
Genius

Hi Bruce.

 

I just had a quick go with what you suggest, I like it.

Betreff: Custom Properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Dazzie, Good. You can also add properties in Prop Man in case you don't notice. Right click a column header, select show properties. Can't delete props though.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: Custom Properties

Honored Contributor
Honored Contributor

Is this the list you are talking about? See attached

 

I call it the annotation list. Some call it callouts because of the name of that menu.

Mine has always sorted alphabetically. 

 

 

Betreff: Custom Properties

Genius
Genius

Hi.

 

With the inventor software I think its within the parts list parameters/properties.

 

It is something that maybe isn't available withing Solid Edge.

 

I will just have to have an extensive library of standard parts.