Cancel
Showing results for 
Search instead for 
Did you mean: 

Custom Wiring Materials and Properties?

Experimenter
Experimenter

I am trying to get an accurate CG and mass for my model as well as accurate lengths for the harnesses. Is there a way to add custom wire types to the drop down list? Like say I want a cable of 30 AWG teflon-coated silver plated copper wires. I want to add that specific density, diameter, and bend radius measurement into the system so that I don't have to go and manually change the bend radius and diameter every time I import wires into the model. Is there a way to create custom wire types so that I can get the properties right when I use the harness wizard?