Cancel
Showing results for 
Search instead for 
Did you mean: 

Custom saved settings in Table properties

Pioneer
Pioneer

Hello

 

I created in drawing environment  my custom table for parts list and saved it as "some name".

Anybody know how to move it beetwen workstations?  I very often make some exercises, settings on workstation at home. I want to have it also at workstation at work. But I don't want to create it form "zero" at work. Where is location of file with saved settings of table properties? I want to copy it and replace on second one workstation.

See attached file to better understand my idea

 

Regards

Marcin

4 REPLIES 4

Re: Custom saved settings in Table properties

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Saved settings are saved to text files in the "..\Program Files\Solid Edge ST##\Template\Reports" folder, so that you can share these files with other users. Parts list saved settings file name is: DraftList.txt.

Re: Custom saved settings in Table properties

Pioneer
Pioneer

Hello Milind

 

Thank You very much for help. It works..Smiley Happy

 

Regards

Marcin

Betreff: Custom saved settings in Table properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,



but You can define a network folder to hold all the TXT files froom reports.

 

Take a look into the options and file locations there should be a line called "reports"

 

Since I'm using a German version of SE I don not knwo exactly the English text for this line.

See the line in the pciture to find it for Your version.

It is the line after the propseed

 

 

20161104_1641.PNG

 

regards
Wolfgang

Betreff: Custom saved settings in Table properties

Pioneer
Pioneer

Thanks Wolfgang.

Your suggestion was also very helpfull for me

 

Regards