02-20-2018 11:11 AM
Hey guys, after running a simulation you can create report. This report only shows Von Mises stress, displacement and safety factor.
It's based on an HTML file in the ResDLL\XXXX (depending on your language in ST10, for me it's "C:\Siemens\Solid Edge ST10\Program\ResDLLs\000C\Static_Study_Report.htm" because I'm french and I installed it in C:\Siemens instead of Program Files). However is there any way to customize this HTML file and get a custom report ?
It seems to use keywords for the result tables and maybe if I generate the image manually with the right name and add the proper sections and keywords in the HTML file it could work ?
Or I will have to write a macro for that ?
Solved! Go to Solution.
02-21-2018 03:18 AM
Aguitton116,
it may be possible to edit the report template,
but I would suggest to add yourself to this Enhancement Request (via your support):
ER#1956754 - Simulation Report content configurable
Good luck,
/Ulf
02-21-2018 03:33 AM
Hi Ulf, technically I'm the guy from the support (because I'm the reseller and you know me because we had some exchange very recently about a simulation case on a pan handle)
Anyway I'm not sure I can add myself to the ER by myself.