Cancel
Showing results for 
Search instead for 
Did you mean: 

Customize Commands

Genius
Genius

Hello,

Have a question here, can we within SE create one button like on the radial menu that would do two things with the click of one button, say it is supposed to save the file then close the file.

 

Or does this have to be like a macro thing setup outside SE



Mervin D. Yoder
CAD | Designing
keimlumber ST9
2 REPLIES

That would need to be a VB macro.

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

That would need to be a VB macro.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: That would need to be a VB macro.

Genius
Genius
Thank you Ken, kind of what I figured.



Mervin D. Yoder
CAD | Designing
Millwork Specialty

[cid:image001.jpg@01CF2414.F6D67770]
Phone:330.893.2251 Ext.339
www.keimlumber.com


Mervin D. Yoder
CAD | Designing
keimlumber ST9