Cancel
Showing results for 
Search instead for 
Did you mean: 

Cut Length Frame in Draft

When doing drawing of Frame model, we can insert  "cut length" properties in the table of part list.
The cut length will be referred to the external length of the frame.

 

Can we change the cut length to be the centerline instead external length of the frame?

 

 

Solid Edge ST9 User.

Window 10

5 REPLIES 5

Betreff: Cut Length Frame in Draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Muhammad_Ayub

 

 

but this might  be dangerous too, if You get wrong length values for the bom?

 

regards
Wolfgang

Re: Cut Length Frame in Draft

Honored Contributor
Honored Contributor

If your wire frame and handle points are the center of the frames.....sure.

Betreff: Cut Length Frame in Draft

@hawcad what you mean by dangerous? which path?

Re: Cut Length Frame in Draft

@12GAGE But all along I use the frame environment, I put the wireframe at the center.

Betreff: Cut Length Frame in Draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Muhammad_Ayub

 

 

the property Cut_Length in a bom shows the outer length of the frame component, maybe with an additional offset for cutting (defined in bom options)

 

If You show the centre length of a frame and there is the need for the overall length it could be, that You get frames, to short for use

 

20170308_1254.PNG

regards
Wolfgang