Cancel
Showing results for 
Search instead for 
Did you mean: 

Cut command now a two step process?

Experimenter
Experimenter

Please forgive me in advance if my terminoligy is a bit off.

Suddenly my cut command is asking that I extend into 2 different directions instead of one.

I want to cut to a finite depth and while the first step allows me to do so, it now asks me to extend in the opposite direction. How can I turn this off and go back to the normal way of cutting? I have no idea how this got turned on.

 Untitled1.pngfirst stepUntitled2.pngsecond step

 

 

5 REPLIES 5

Re: Cut command now a two step process?

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Turn of the non-symmetric extent option.

 

Capture.JPG

Highlighted

Re: Cut command now a two step process?

Experimenter
Experimenter

Thank you. That worked.

Betreff: Cut command now a two step process?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @dcoleman

 

 

 

You nearly can answer Yourself when looking onto Your pictures.

You can see the reason for that, and this is that You have turned on the  "Non-Symmetric Extend" option!

 

20180628_1909.png

 

 

Just turn it OFF and everything will work as before!

 

regards
Wolfgang

Betreff: Cut command now a two step process?

Experimenter
Experimenter

Thank you! I swear I clicked that intending to turn it off. Maybe I was trying to do it too quickly and overlooked it.

Right under my nose!

Betreff: Cut command now a two step process?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello @dcoleman

   

Please mark one or more messages as 'accepted solutions'

It will make easy for users reading this discussion in future to find out the solution quickly, instead of reading through all messages.

   

Thanks.