Cancel
Showing results for 
Search instead for 
Did you mean: 

Cut text in part takes long time

Creator
Creator

Dear Members,

 

I want to create a data plate for a device in which the text is cut out. My problem is that any modifications on the part, when the part redrawn, are taking a lot of time (5 mins, and only one word is cutted out yet). Is this normal? See the attached picture for the texts.

Are there any methods for creating texts on a part which can be shown on draft drawing?Data_table.jpg

2 REPLIES

Re: Cut text in part takes long time

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @magiclevinho,

 

Are you sure you want them cut out? [I pressume THAT is the part that takes a long time to process]....or is that so you can get them to show in the draft?

 

You could leave it as a "Sketch" in the plate model, or also, in Sheet Metal you can use the "Etch" command, which is then suitable for laser etching, etc.

Both of these methods can easily be displayed in the draft, via the view properties, select the "Parts List Option" button to see all options, click on the sketch you want to display in that view, and check the box to "Show".....you should be good to go.

 

2017-03-20.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Cut text in part takes long time

Creator
Creator

@SeanCresswell

Thank you! I thought I will have to cut it, but it is not neccessary, as long as I can show it in the drawing.

Thank You again!