Cancel
Showing results for 
Search instead for 
Did you mean: 

Cutting Plane Leader and Terminator Lenght

Experimenter
Experimenter

Hello,

 

Could you please help me on this issue.

 

I would like to change the (B) length of a Cutting Plane (Please refer to the image below) to a shorter dimension. However I do not want terminator length (T)  to be changed and also I do not want to draw for my self the cutting plane geometry as a group or as a block. Is that possible?

 

Thanks.

 

Rogerio

cutting_Plane_leader.JPG

cutting_plane.jpg

 

 

 

3 REPLIES
Highlighted

Re: Cutting Plane Leader and Terminator Lenght

Phenom
Phenom

Just grab hold of the end of the leader line and drag it shorter or longer.

I notice you appear to have 2 different positions of section arrow, one pointing away from the section line, the other away from it.

In the top one you would drag the non-arrow end.

I think in the bottom one you would drag the arrow end.

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.

Re: Cutting Plane Leader and Terminator Lenght

Siemens Phenom Siemens Phenom
Siemens Phenom

You can simply click and drag on the end ot the terminator line away from the cuting line to lengthen or shorten it.

Regards,

Rick B.

Re: Cutting Plane Leader and Terminator Lenght

Experimenter
Experimenter

That´s it. Thanks a lot.