Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Cutting Plane Properties

Valued Contributor
Valued Contributor

OK. I am sure this is simple but...in Draft, I have my cutting plane properties to use a 0.35mm line. But when I add a cutting plane it comes through at 0.46mm which is often much too thick. Any idea of how I can get it to be 0.35mm?

I can post some pictures if that helps.

Regards

Peter Smith

3 REPLIES

Re: Cutting Plane Properties

Genius
Genius

Hi @Greybarn Create a new drawing view by modifying the size of the line, check the video.

 

Thanks.

(view in My Videos)

Regards.

Re: Cutting Plane Properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Greybarn

 

 

 

as shown by @Kanwulf video You can change and define  the style of every object in Your draft.

 

But to get them also for every new drawing You will create, You have to define that inside Your templates rather then changing it again and again.

So define Your wanted styles in Your template draft and from than on it will be no doubt that your drawings will look like as You expected them to do.

 



regards
Wolfgang

Re: Cutting Plane Properties

Valued Contributor
Valued Contributor

Thanks for that. I was able to get that to work for me.

Regards

Peter