Cancel
Showing results for 
Search instead for 
Did you mean: 

Cutting Planes and attaching to geometry

Pioneer
Pioneer

I am making a cutting plane through a cylinder to show hole work in it.  Whenever the diameter of the cylinder changes (either grows or shrinks) on my solid model, then the cutting plane wont cover my holes anymore.  Is it possible to attach a cutting plane to geometry so that if the geometry changes then the view can "keep up" with it?

1 REPLY 1

Re: Cutting Planes and attaching to geometry

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

You probably needed to post this in the SE Forum, rather than the SE 2D Drafting......but, to answer your question, yes you can, you just need to place some relationships on the cutting plane sketch to keep it relevent to the model geometry.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000