Cancel
Showing results for 
Search instead for 
Did you mean: 

Cutting a section in ST5 Free2d?

Creator
Creator
I am trying to locate how to create a section in Free2D ST5. I have found information on Cutting Plane, but it seems as though these function are disabled. Is there an icon in one of the menus that allows you to put section marks on the drawing without having to draw the section lines and add the text and draw an arrowhead manually?
1 REPLY

Re: Cutting a section in ST5 Free2d?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi there, As far as I'm aware, this functionality is "only" used based on having a 3D file to cut sections through....I believe the tool is "disabled" only because of this...and is not different to commercial & academic versions, if there was no 3D data to reference for sectioning. 2D views (sections, or otherwise) will all be unique, as in other 2D apps.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019