Cancel
Showing results for 
Search instead for 
Did you mean: 

DATA EXTRACTION FROM D3 PART MODEL

Experimenter
Experimenter

Hi,

I just wanted to know that the data which is fed into while creating holes on the 3D model can it be extracted completly,

Example: In the hole Command while selecting it ask for different types of options like ,Standard,Size,type of hole,etc.

suppose in which i feed the data in the following manner.

 

                                       Standard-ANSI Inch

                                       Size;-1/4"unc,etc

 

Now from above fed data i am interested in knowing whether the above details can be refelcted in the draft environment of that particular part or not.

1 REPLY 1

Re: DATA EXTRACTION FROM D3 PART MODEL

Gears Phenom Gears Phenom
Gears Phenom

YES,

 

in the Draft, find the Call Out command,  within you will find Hole Callout  which will annotate the 3D Hole. 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7