Cancel
Showing results for 
Search instead for 
Did you mean: 

DDM in SE ST10

Experimenter
Experimenter

Hi,

I have a problem with DDM in SE ST10.
I can not have automatic Windows updates enabled.
After updating, windows DDM in SE does not work correctly.
I need to reinstall DDM.
Do you know how to fix it?

8 REPLIES 8

Betreff: DDM in SE ST10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Tadeusz

 

 

 

 

this for me more sounds to be an issue by DDM rather than SE.

 

So I better would ask the DDM  people. 

 

 

regards
Wolfgang

Betreff: DDM in SE ST10

Gears Phenom Gears Phenom
Gears Phenom

@Tadeusz   as @hawcad suggest's...  this seems like an issue that needs to be addressed by DDM.   They have great support directly at ddm.support@design-simulation.com

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Betreff: DDM in SE ST10

Experimenter
Experimenter

Hi,

I want help for DDM in SE ST10 - Design Data Management.

DDM is a PDM/PLM solution.

Betreff: DDM in SE ST10

Siemens Phenom Siemens Phenom
Siemens Phenom

@Tadeusz DDM is a third party product and is not a Siemens PLM product:

 

http://www.designdatamanager.com/solutions/solid-edge-plm/

 

The Siemens PLM Solid Edge data management products are:

 

  • Built In Data Management (BiDM)
  • Teamcenter Client for Solid Edge (SEEC) 
  • Solid Edge for SharePoint (SESP)
  • Insight 

 

If you question is related to one of the above four products then you ae in the right place.  Otherwise, issues related to the DDM product are best addressed with that third party. 

 

 

Betreff: DDM in SE ST10

Experimenter
Experimenter

Hi,

I have a Built In Data Management (BiDM).

My reseller name it DDM.

My reseller can not help me.

According to him, I need to disable automatic Windows updates.

Otherwise, after the automatic Windows updates, BiDM stops working on some computers.

Betreff: DDM in SE ST10

Siemens Phenom Siemens Phenom
Siemens Phenom

@Tadeusz obviously I do not know the specifics yet of your issue but I would like to discuss and engage with you further on this offline.  I have sent you a PM.  Please respond to that message.

 

For the rest of the community, after I have engaged directly with @Tadeusz and understand the issue better I will report back here.  The comments such as "disable Windows Automatic Update or BiDM stops working" needs to be clarified for all.

Betreff: DDM in SE ST10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Tadeusz  If you are in fact using BiDM, then there is a known issue where some Windows updates unregister the Solid Edge file properties from the Windows Search Service.  The repair requires the SEPropertyHandler.dll file to be reregistered.  I'm not sure if this issue has been resolved in a patch yet, but it seems that we have not seen the issue for some time now.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: DDM in SE ST10

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @KennyG

 

 

 

I also must say that this issue now did not appear for a long time!

 

So it seems that it was fixed somehow with a MP of Solid Edge

 

regards
Wolfgang