Cancel
Showing results for 
Search instead for 
Did you mean: 

DIMESION OPTIONS -DISTANCE BETWEEN KEYPOINTS

Pioneer
Pioneer

Dear all,

I am looking for, how to change setting for dimension between keypoints.

 

Solid edge--ST7-- Assembly--PMI--dimension--smart dimension--dimesion between keypoints

 

Its always setup on center and endpoints.

My question is, how can i setup to all endpoints as my default setting?

 

 

4 REPLIES

Re: DIMESION OPTIONS -DISTANCE BETWEEN KEYPOINTS

Honored Contributor
Honored Contributor

I sugest trying the point to point dimension rather than smart dims. This solved a few of my problems when I started using it. It is a slower tool most of the time, but when you need it, it's there.

Re: DIMESION OPTIONS -DISTANCE BETWEEN KEYPOINTS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

Use the "Distance Between" tool instead, then select "By 2 Points" from the orientation drop down....and you can also isolate select entity types, with the "Keypoints" filter.

 

SE_ST7_Assy_PMI_DistanceBetween[By2Points].png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: DIMESION OPTIONS -DISTANCE BETWEEN KEYPOINTS

Pioneer
Pioneer

Thank you for responses but I think my point is different. 

My question is how to set up my preference of keypoints to "all" instead of "center and endpoints" as default so that i dont have to keep changing it. please check image.

Re: DIMESION OPTIONS -DISTANCE BETWEEN KEYPOINTS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I do not believe there is a way to do this.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com