Cancel
Showing results for 
Search instead for 
Did you mean: 

DOWNLOAD SOLID EDGE MAC OS X

Experimenter
Experimenter

Good day,

 

I'm new to the forum, I want to know how to download SOLID EDGE for MAC Student License.

4 REPLIES 4

Re: DOWNLOAD SOLID EDGE MAC OS X

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Microsoft Windows (x64) only.  There is no version for OS X...



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: DOWNLOAD SOLID EDGE MAC OS X

Experimenter
Experimenter

Thanks, for your support.

 

exist an old version for mac, available?

Re: DOWNLOAD SOLID EDGE MAC OS X

Gears Phenom Gears Phenom
Gears Phenom

NO,  your best bet is something like bootcamp tha will allow you to boot into a Windows OS environment and then you can install SE.

 

See prior thread:   https://community.plm.automation.siemens.com/t5/Solid-Edge-Student-Edition-Forum/is-sold-edge-avail-...

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: DOWNLOAD SOLID EDGE MAC OS X

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@IvanPenagos  Solid Edge has never been available for Mac OS X.  It has always been a Microsoft Windows only application.  As @Johnson_BigMatt said, if you want to run it on a Mac, you must use a utility (BootCamp) that allows you to install and boot into a Microsoft Windows installed partition.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com