Cancel
Showing results for 
Search instead for 
Did you mean: 

DWG to sketch in part

Experimenter
Experimenter

Hello,

 

I need to add some logo's on a part, i have these logos in dwg/dxf. I was wondering if it is possible to inport these dwg files to a sketch within the part file. With these sketches would want to make an extrusion.

 

Thanks in advance,

 

Ruben

2 REPLIES 2
Highlighted

Re: DWG to sketch in part

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello Ruben,

 

Yes, this is possible.

Start the Open command and select the DWG/dxf file you have.

This will open the drawing in a draft document.

You can simply copy the logo objects from draft and paste it into the sketch for further extrusion.

 

Alternatively, if you click the Options button while still in the File Open dialog, a wizard opens which will present option to directly open the drawing in a part sketch.

 

Here's a video of the steps:

https://www.youtube.com/watch?v=dPj2lhv7cis

 

Regards,

Tushar

 

Re: DWG to sketch in part

Experimenter
Experimenter

Thanks! Worked as a charm.