Cancel
Showing results for 
Search instead for 
Did you mean: 

Dan,    I do also have problems with importing from AutoC...

Experimenter
Experimenter

Dan, 

 

I do also have problems with importing from AutoCAD (.dwg format). After I click the Finish button in the Options wizard, I only get a blank draft page. Nothing has been imported. Could it be that I am running the educational version of Solid Edge (ST5) and also an educational version of AutoCAD (2014 version). Thanks in advance! 

1 REPLY 1

I do not believe that ST5 is able to translate AutoCAD 20...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I do not believe that ST5 is able to translate AutoCAD 2013/2014 files.  That capability was added to ST6.  You would need to save your DWG as an older version...



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com