Cancel
Showing results for 
Search instead for 
Did you mean: 

Dashed lines on coordinate dimensions

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Hello,

 

Has anyone seen these dashed lines before?  Our other designer noticed these on a couple of coordinate dimensions including a zero datum dimension:

 

Coordinate Dotted Lines Markup.jpg

Kyle Joiner
IPA LLC
ST10 MP1
15 REPLIES 15

Betreff: Dashed lines on coordinate dimensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @kjoiner

 

 

no, not until now when You share Your pictures.

 

What, if You use a different (standard) template for draft and reset Your user options (renaming registry)?

 

 

regards
Wolfgang

Re: Dashed lines on coordinate dimensions

Phenom
Phenom

I saw these the other day for the first time and was very surprised they printed.

 

I ultimately went into the drawing and moved the dimensions around a bit to make them go away and then located the dimension back in the position I desired. 

 

It was a one time deal and I have not seen them since.

 

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Dashed lines on coordinate dimensions

Gears Phenom Gears Phenom
Gears Phenom

they look to be created due to a jog...  but that doesnt make sense completly for the origin.

or amybe an alignment indicator of some sort...  but again  why are they same color as dim and printing?

 

HMMM...

 

 

following...

 

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Dashed lines on coordinate dimensions

Phenom
Phenom

They appear when you select a dimension, including the origin, without jogs. Normally they turn off when you deselect the dimension. However, in what seems like rare cases, they stay on and will print. As I said, I have only seen this happen once. It appears they have something to do with dimension alignment.

 

2017_05_22_15_51_22_Solid_Edge_ST9_Draft_Draft2_.png

Bob Henry
REH Technical Consulting
Canonsburg, PA 15317

Re: Dashed lines on coordinate dimensions

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Hello,

 

I'm not the only one seeing this.  Would a reboot help?

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Dashed lines on coordinate dimensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @kjoiner,

 

I've seen this issue also, and seems to be local to the file, so a Solid Edge, or even a system, reboot doesn't reset it.....until the location nudging happens, and the indicator line is then gone.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Re: Dashed lines on coordinate dimensions

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

what graphic cards are You using?

 

 

regards
Wolfgang

Re: Dashed lines on coordinate dimensions

Legend
Legend

They appears and disappear randomly in my case.

Héctor Pelayo Izquierdo
Engineering Department, JAE Ingeniería y Desarrollos, S.L.
Solid Edge ST9 MP5 | NX 9
Development: VB.NET

Re: Dashed lines on coordinate dimensions

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

My computer and the one having the issue are both using nVidia Quadro 2000 cards.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1