Cancel
Showing results for 
Search instead for 
Did you mean: 

Datum Frames Properties

Creator
Creator

is it possible to change the default settings for " Datum Frame Properties" and how?

1 REPLY 1

Betreff: Datum Frames Properties

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Rebel_za 


Datum Frame settings are also a matter of the used Format Style
So if You define different format styles (like ISO_Bezug and ISO) in my example - the differ in font size and color) You can use them for creating certain elements

And You can use the option for Dimension Style Mapping to automatically use certain styles for certain elements

But take care that this is done in the template draft file to have that in use for all future documents
And You can organize such format style to copy them to old documents too

regards
Wolfgang