Cancel
Showing results for 
Search instead for 
Did you mean: 

Decimal Precision for Non Graphical Parts

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Hello,

 

I am including some label sheets for an assembly.  In the past, I have used non-graphical parts for wire lengths etc. and it seems SE defaults to two decimal place precision.  For the label sheets, I just want to show the integer.  What do I enter in the custome properties to show that?

 

Thanks,

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1
4 REPLIES 4

Re: Decimal Precision for Non Graphical Parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You mean for display in a parts list, right?

Maybe this will help?

https://docs.plm.automation.siemens.com/tdoc/se/108/help/#uid:ngrphc2h

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Decimal Precision for Non Graphical Parts

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Thanks Bruce,

 

That worked.

 

I only do these every few years and my memory fades.  This is something SE could make a little more "user friendly".

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Decimal Precision for Non Graphical Parts

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Ditto

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Decimal Precision for Non Graphical Parts

Phenom
Phenom

My tip for this is to create template files for the 2 types of non-graphic parts.

It would also be nice if the number of decimal places and units could be specified for other things such as lengths of frames, tubes etc. and have them round up or down as required.

Specifying a quantity of 4281.25mm for a length of a rubber seal just doesn't look good (and it doesn't fit the quantity column in our parts lists). I want to be able to show 4.5 or 5m.

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.