Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Default Bend R

Honored Contributor
Honored Contributor

Context: Sheet metal part, Ordered, Assembly driven part:

 

I'm wondering if there is a way to keep the "Default bend radius" box checked. Every time I start a new flange, I have to go check that box. I want to keep it checked all the time. To me, this is the purpose of a "Default bend R" but I have to go make it the default many times as I create a model.

 

One step beyond that, What controls what shows up in the box before that box is checked?

2 REPLIES 2

Re: Default Bend R

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

"Save Default" button on bottom right of Flange Options dialog.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Default Bend R

Honored Contributor
Honored Contributor

This one was a "Doh" once I looked at it more closly.