Cancel
Showing results for 
Search instead for 
Did you mean: 

Default Flat Pattern (dxf)Directory ?

Creator
Creator

Am wonder if there is a way to set a default flat pattern directory. I am using BIDM and by default 

my flat patterns want to save at the in process location with no respect to any folder structure.

     I have a flat pattern directory outside the Vault that has the same folder structure as the Vault.

We chose to not have flat patterns in the Vault do to the fact that we get flat pattern files (dxf)

from customers.   

 

               Or does someone have a macro for this type of thing.

 

16 REPLIES

Betreff: Default Flat Pattern (dxf)Directory ?

Esteemed Contributor
Esteemed Contributor

Hi @Milro

 

 

You can use my SheetLaser macro which allows many methods for defining the dxf folder 

 



regards
Wolfgang

Betreff: Default Flat Pattern (dxf)Directory ?

Creator
Creator

@hawcad

           I am looking into this, it  looks like it might be my answer . I am struggling to get it set up . Do you

have an english instruction guide and does it allow UNC paths?

 

Betreff: Default Flat Pattern (dxf)Directory ?

Esteemed Contributor
Esteemed Contributor

Hi @Milro

 

 

 

Yes it allows UNC pathes and if You look into the INI fiule, there should be English explanations too!

 

20180329_1337.PNG

 

 

 

And You further also can use my MainDim macro which will have the SheetLaser as integrated part, but also is doing a lot more for You regarding main dimensions, properties, etc.

 

 



regards
Wolfgang

Betreff: Default Flat Pattern (dxf)Directory ?

Creator
Creator

@hawcad

            I have the maindim macro but don't have the ini file you are talking about could you share 

a link to the sheet laser download site ?

                        Thank You

Betreff: Default Flat Pattern (dxf)Directory ?

Esteemed Contributor
Esteemed Contributor

HI @Milro

 

 

with the "newer" MainDim macro I have changed all setting into the XML file

 

 



regards
Wolfgang

Betreff: Default Flat Pattern (dxf)Directory ?

Creator
Creator

@hawcad

       I almost have it working but am stuck on the syntax for project . I am getting this error 

error.JPG

xml.JPG

also for some reason the maindim is unexposing a my H variables.

Betreff: Default Flat Pattern (dxf)Directory ?

Esteemed Contributor
Esteemed Contributor

HI @Milro

 

 

is it possible to upload the specific PSM file or to send it via PM

 

 



regards
Wolfgang

Betreff: Default Flat Pattern (dxf)Directory ?

Creator
Creator

@hawcad

           Yes here is the file that I am using as a test.

Betreff: Default Flat Pattern (dxf)Directory ?

Esteemed Contributor
Esteemed Contributor

Hi @Milro

 

 

and if possible Your two XML options files also

 

I believe that here is some syntax problem or similar

 

Thanks in advance

 

 



regards
Wolfgang