Cancel
Showing results for 
Search instead for 
Did you mean: 

Default colors

Experimenter
Experimenter

How can I change the default colors for dimensions, annotations, etc?  My printer doesn't like the default blue.

5 REPLIES

Re: Default colors

Gears Phenom Gears Phenom
Gears Phenom

you are looking for "Styles" and will need to change these in your template.

 

DIMENSION STYLE in this case...

 

BUT,  also not that there is an option to print all colors as black as well, if you can get by with a BW print.

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Default colors

Experimenter
Experimenter

Where do I find "styles"? I have the 2D free.  Yes, I can print in B&W but the blue shows up lighter.  I'd like to just have plain ole black.

Re: Default colors

Experimenter
Experimenter

I think I found it

Re: Default colors

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@MikeByrd

 

If you use the Solid Edge print dialog's "Print all colors as black", it forces all colors to black rather than grayscale thus not requiring you to change your colors...  This is what @Johnson_BigMatt was referring to.

 

If you use your printer's Properties setting of Black & White, then it will print colors other than black as grayscale.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com

Re: Default colors

Experimenter
Experimenter
Thanks