Cancel
Showing results for 
Search instead for 
Did you mean: 

Defining blok distance on draft background

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello everyone,

Need help on how make a distance for template from background sheet.

 

 

Capture.JPG

 

Thanks

Destian

2 REPLIES 2

Betreff: Defining blok distance on draft background

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


supposing You are talking about the red objects on Your background sheet

 

Use RMB and properties to enter the coordinates etc for the selected element (in this case itmight be lines)

 

Other method I have used very often is to put a circle on the background sheet, using above method to put it on 0,0 and give it a fixed geometry relation

 

Than You can use this circle for dimensioning the rest

 

 

regards
Wolfgang
Highlighted

Betreff: Defining blok distance on draft background

Honored Contributor
Honored Contributor

As a starting point, add a circle to 0,0

 

Once you get everything where you want it, ground it and delete the circle.