Cancel
Showing results for 
Search instead for 
Did you mean: 

Defining the Custom Occurence Property

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

assuming the new ST9 fetaure of a Custom Occurence Property within assemblies I have seen that theer alsso seems to be the possibility to define lists for those Occurence Properties.

But I haven't sen any description or definition of the form of that list entries.

 

Tried several syntax of HTML, XML, semicolon and so on but all of them brought no proper result.

 

Any hints or ideas?

 

Thanks in advance

 

regards
Wolfgang
8 REPLIES

Re: Defining the Custom Occurence Property

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Wolfgang,

 

All custom properties must be contained in an XML file defined in Solid Edge Options/File Locations/Custom Occurrence Property File (Program/Preferences/CustomOccurrenceProperty.xml by default). If you look at CustomOccurrenceProperty.xml that is delivered, it describes the format as well as a few example properties that will show you how to create the properties. For the list scenario, look at the 'Maintenance' property that is an example property in the file:

 

<OccurrenceProperty>
    <Name>Maintenance</Name>
    <Description>Specifies the maintenance schedule for the component (Can be overridden from upper level) (Global+Overrides)</Description>
    <PropertyBehavior>Global+Overrides</PropertyBehavior>
    <ListOfValues>
        <Value></Value>
        <Value>Daily</Value>
        <Value>Weekly</Value>
        <Value>Bi-Weekly</Value>
        <Value>Monthly</Value>
        <Value>Quarterly</Value>
        <Value>Yearly</Value>
    </ListOfValues>

    <DefaultValue></DefaultValue>

</OccurrenceProperty>

 

The first value in the example list of values will give you a blank entry.

 

Hope this helps,

Greg

Re: Defining the Custom Occurence Property

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,


Thanks a lot - works fine!

 

<Value> was the mistake!

 

regards
Wolfgang

Re: Defining the Custom Occurence Property

Siemens Phenom Siemens Phenom
Siemens Phenom

Great!

Re: Defining the Custom Occurence Property

Hi,

 

thanks for the explanation of the XML file.

But is there a GUI friendlier setting for this? Like the options.xml tool (SEadmin)?

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Defining the Custom Occurence Property

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Daniel,

 

Unfortunately there is not.

 

Greg

Re: Defining the Custom Occurence Property

Smiley LOL

Funny, new custom interface but no GUI. Lets do a propseed work method then.

-------
Daniël Schuiling
Solid Edge ST7
Teamcenter 10

Re: Defining the Custom Occurence Property

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@GregLuckett, just a comment: the path you give makes no sense to me. Mine is in the preferences folder. Don't even have a "common" folder.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Defining the Custom Occurence Property

Siemens Phenom Siemens Phenom
Siemens Phenom

@bshand, sorry about that, you are correct. It is in the 'Preferences' folder in the program directory. I was thinking in terms of a development build... I fixed it in the other post.

 

Greg