Delete Error

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I have SE installed... I noticed the delete does not delete. Set the delete icon to radius menu. Delete goes back to assembly from the Create and Edit. Also, the same goes for sync part. I checked the SE options nothing.

Thanks Greg

10 REPLIES

Re: Delete Error

Esteemed Contributor
Esteemed Contributor
Not totally clear on what your asking here....

Delete works perfectly for me...although, not tried [bothered] putting it on the radial menu.
Not 100% sure until I get to a system with it loaded, but does Student Edition actually let you save the new customised theme's?
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Delete Error

Phenom
Phenom
Greg, are you trying to delete a document? A line or arc element in a sketch? Are you in the sketch when you do this? Is the element selected and highlighted?
-Dylan Gondyke

Re: Delete Error

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor
I noticed when I opened SE for the first time after installation, the
delete was not on the Radial Menu. However, I was able to use delete in the
previous installation.This installation was not included... Also, the
default is set without the delete So, I changed to my settings... drag
delete to the radial menu amungst others.
I have Jing installed to show a video or snapshot, and cannot show the true
movement. While using the delete on the radial menu goes from sync part to
assy. I have to use the delete key on the keypad instead.

Thanks
Greg

Re: Delete Error

Phenom
Phenom
Greg, I think you might have accidentally dragged the Close and Return or Exit Environment button onto the radial menu and NOT the delete button.
-Dylan Gondyke

Re: Delete Error

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor
I believe I did use the delete/ Close button. The original default did not
include the delete button at all.

Thanks
Greg

Re: Delete Error

Phenom
Phenom
Perhaps if you took a picture of your radial menu and posted it here, or took a short video of the behavior? There isn't much more we can do to help you without one of those things.
-Dylan Gondyke

Re: Delete Error

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor
Hi Chally72,
This short video hopefully will help you understand with the issues on
this Radial Menu on the delete icon and close.
Thank You
Greg

Re: Delete Error

Esteemed Contributor
Esteemed Contributor
What short video?

Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: Delete Error

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor
Try this attachment... Works well with Quick Time Player