Cancel
Showing results for 
Search instead for 
Did you mean: 

Delete, or not...

Gears Phenom Gears Phenom
Gears Phenom

When starting a new project from an existing project I open the main assembly and make changes to the properties with the properties manager.

 

Changes are OK, but when you delete, it's not kept...

https://www.youtube.com/watch?v=WLcXx6tEHEw

 

I can delete, but after closing an reopen, the old (wrong) quantity is there again.

 

I want the quantity (custom property) deleted, I will fill this in later.

Is this behaviour as wanted??

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user
18 REPLIES

Re: Delete, or not...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I never use a custom property for quantity but I did create one in a part used in an assy. When I use prop mgr on that assy changing the number did stick as you would expect. Don't know what's happening with you.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Delete, or not...

Gears Phenom Gears Phenom
Gears Phenom

A change to an other number is indeed no problem.

Deleting to "empty" however doesn't stick.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Delete, or not...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Maybe because it's a numeric property. Will zero "0" work? Or a dash. Or period. Or ?

 

Edit: It should work if it's a text property. Is text acceptable?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Delete, or not...

Gears Phenom Gears Phenom
Gears Phenom

Everything is acceptable because I will change the value during the calculation of the project, but I want to chang it only for the 'this project only'-files. All the rest (company standard parts, hardware,...) needs to stay empty.

So 1 hit on the delete key is fast and what I want, but SE doesn't work with me...

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Delete, or not...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think a numeric property needs a value of some kind, even "0".

 

You can make the value 0 or change the property type to text.

 

You can copy and paste many fields at once if that helps.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Delete, or not...

Gears Phenom Gears Phenom
Gears Phenom

I will use this workaround, but still hoping I wil once be able to silmpy hit the Delete button. Man Wink

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Delete, or not...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Not likely with a numeric property type.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Delete, or not...

Gears Phenom Gears Phenom
Gears Phenom

Strange because:

At start this is empty without a problem and second: It is a "text" property.2016-02-23 08_20_00-Rughaak_Rechts.psm Properties.png

 

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Delete, or not...

ithink you will need to replace the exsting value with a "space"

 

i do not think you can delete but have to have some other value in there...