10-26-2017 02:55 PM
I have working on this one till I got a headache.
I have this hinge and I need to make a left and right hinge because if you try to install it on the left, the screws are on the wrong orientation.
The right side is easy.
I noticed that within the part there are several pieces that are grounded and I do not see where they are grounded.
Am I missing something?
Solved! Go to Solution.
10-26-2017 03:08 PM - edited 10-26-2017 03:11 PM
There are two subassemblies each of which has parts inside which are grounded. Open both subs and you will see the ground relations on the parts.
Edit: And one of the subassemblies is grounded inside the main assembly.
10-26-2017 03:10 PM - edited 10-26-2017 03:13 PM
Hi there @Lex-luthor,
No need to delete the existing relationships......If you make the hinge sub-assembly "adjustable", you can set the orientation how you want, and will allow that swivel function as such. Then use "Drag Component" command to rotate it.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000
10-26-2017 03:14 PM
Sean actually opened to the topmost assembly whereas I did not.
10-26-2017 03:19 PM
10-26-2017 03:38 PM - edited 10-26-2017 03:38 PM
@Lex-luthor, Sean is also known as Superman around here.
10-26-2017 03:43 PM