Cancel
Showing results for 
Search instead for 
Did you mean: 

Deleting Ground Relation In a Part

Valued Contributor
Valued Contributor

I have working on this one till I got a headache.

 

I have this hinge and I need to make a left and right hinge because if you try to install it on the left, the screws are on the wrong orientation.

 

The right side is easy.

 

I noticed that within the part there are several pieces that are grounded and I do not see where they are grounded.

 

Am I missing something?

 

 

6 REPLIES 6

Re: Deleting Ground Relation In a Part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There are two subassemblies each of which has parts inside which are grounded. Open both subs and you will see the ground relations on the parts.

 

Edit: And one of the subassemblies is grounded inside the main assembly.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Deleting Ground Relation In a Part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Lex-luthor,

 

No need to delete the existing relationships......If you make the hinge sub-assembly "adjustable", you can set the orientation how you want, and will allow that swivel function as such. Then use "Drag Component" command to rotate it.

 

ST10_ASM_AdjustableAssembly.PNG

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Deleting Ground Relation In a Part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Sean actually opened to the topmost assembly whereas I did not.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Deleting Ground Relation In a Part

Valued Contributor
Valued Contributor

@SeanCresswell

 

You Rock Sir!

 

I did not think of that!

 

Thank you. 

Highlighted

Re: Deleting Ground Relation In a Part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Lex-luthor, Sean is also known as Superman around here.

Bruce Shand
SE2019 MP8 - Insight - Win10 - K4200

Re: Deleting Ground Relation In a Part

Valued Contributor
Valued Contributor

@bshand

 

Im glad that he's on our side!  HAHAHA